AXIS#.MOTOR.TEMP
Description
This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.
Context
For more information see Motor and Motor Temperature View.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Ω |
Range |
0 to 232 Ω |
Default Value |
N/A |
Data Type |
Integer |
See Also |
N/A |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Fieldbus Information
FieldbusA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDOPDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.MOTOR.TEMP | 0x500B | 0x2 | UDINT | - | - | RO | True |
AXIS2.MOTOR.TEMP | 0x510B | 0x2 | UDINT | - | - | RO | True |