AXIS#.VL.FB
Description
AXIS#.VL.FB returns the velocity feedback as it is received in the velocity loop after passing through Filter 3 and Filter 4.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read Only |
Units |
Depends on AXIS#.UNIT.VROTARY (pg 1) Rotary: rpm, rps, deg/s, (custom units)/s, rad/s |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics