AXIS#.WS.DISARM

Description

This command disables wake and shake immediately. Feedback type is not relevant for this command. If AXIS#.WS.ARM has been issued, the request to execute the wake and shake algorithm at the next enable is cancelled. AXIS#.WS.STATE is set to IDLE.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Command

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

See Also

N/A

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Related Topics

Wake and Shake Overview