EEO#.LINES
Description
Sets how many lines are output for one revolution of the source feedback. When configured to output CW/CCW or step/dir signals (EEO#.MODE 1 or 2) you will get 4 times this value of pulses per revolution.
Examples
Code
This will set the number of EEO2 lines to 8096.
-->EEO2.LINES 8096
Context
For more information see Encoder Emulation.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 0 to 16777215 |
Default Value | 1024 |
Data Type | Integer |
See Also | |
Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.