A queuing mechanism is provided for all PLCopen A vendor -and product- independent worldwide association active in Industrial Control and aiming at standardizing PLC file formats based on XML motion function blocks including single-axis and master/slave moves. This mechanism allows the application to queue a next move while the active move is executing. The buffer modes, described below, define the transition from the active move to the next move.
See Also
Stay Connected with Kollmorgen
Copyright © 2021 Kollmorgen