Editable PDOs

This section lists all of the PDOs which may be edited. PDOs may be created (Add PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices.), modified (Edit PDO), or removed from the project (Delete PDO). Please see the EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs device-specific documentation for more details.

The Input (Tx) and Output (Rx) PDOs are grouped separately. Each PDO table contains the following information:

Index Identification value for the PDO. The range is defined by the EtherCAT specification.
RxPDOs: 0x1600 to 0x17FF
TxPDOs: 0x1A00 to 0x1BFF
Name Text label to identify the PDO. The name is provided either by the device vendor or user, and can be changed by the user.
Size [bytes] Total length for the PDO object(s) data.
User Modified Yes: indicates the user has changed the PDO or its content
No: indicates the PDO is the default provided by the device vendor.

The KAS IDEClosed "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger compiler enforces restrictions on the sizes of individual PDOs as well as on the sum of the sizes of PDOs. See PDO Restrictions and Compiler Errors for more information.