| Restore Controller |
This function restores a AKD PDMM or PCMM's firmware, network configuration, retained variables and application from the SD card. |
| Restore Devices |
This function automatically restores the data and firmware of any replaced AKD or AKD2G drives, and the station alias of other EtherCAT devices. |
| Advanced |
Clicking this button creates a map of the network and it's components. If a valid firmware file is found and the current topology matches the backup file you may select the device(s) that need to be restored. Clicking Restore selected devices will restore the drive's firmware.
 |