AOUT#.VALUE

Description

AOUT#.VALUE reads the analog output value.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range 0 to 10V
Default Value 0V
Data Type Float
See Also  
Stored in Non Volatile Memory No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AOUT1.VALUE 0x3800 0x1 INT 1000:1 - RO True
AOUT2.VALUE 0x3801 0x1 INT 1000:1 - RO True