AXIS#.IL.COGCOMP.TEACH.POSEND
Description
The end position needed during the Cogging Compensation teach to stop after passing the cogging compensation table maximum position.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-08-00-000 |
General Information
Type |
Read Only |
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
Range |
Depends on units. See Position Range for details. |
Default Value | 0 |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.