AXIS#.IL.COGCOMP.TEACH.STATUS

Description

The status of the Cogging Compensation teach phase.

Versions

Action Version Notes
Implemented 02-08-00-000

General Information

Type

Read Only

Units

N/A

Range

0 - Cogging compensation in not running.

1 - Cogging compensation teaching algorithm is running

2 - Cogging compensation table has been successfully created

100 - Cogging compensation encountered an error while teaching

Default Value 0

Data Type

U8

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.ILClosed "Instruction list" This is a low-level language and resembles assembly.COGCOMP.TEACH.STATUS 0x500A 0x22 USINT 1:1 - RW False
AXIS2.IL.COGCOMP.TEACH.STATUS 0x510A 0x22 USINT 1:1 - RW False