AXIS#.IL.FOLDFTHRESHU

Description

AXIS#.ILClosed "Instruction list" This is a low-level language and resembles assembly.FOLDFTHRESHU is set by the user as the fault threshold of both motor and drive foldback algorithms. The actual threshold value, namely AXIS#.IL.FOLDFTHRESH , is the minimum of AXIS#.IL.FOLDFTHRESHU, AXIS#.IPEAK and AXIS#.MOTOR.IPEAK .

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to 500 Arms

Default Value

Drive peak current (IPEAK)

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.FOLDFTHRESHU 0x500A 0x9 DINT 1000:1 - RW False
AXIS2.IL.FOLDFTHRESHU 0x510A 0x9 DINT 1000:1 - RW False