AXIS#.IL.LIMITN

Description

This parameter sets the negative user limit clamp value of the torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist-producing q-component current command (AXIS#.IL.CMD ). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

Negative drive peak current (IPEAK) to 0 A

Default Value

Negative drive peak current (IPEAK)

Data Type

Float

See Also

AXIS#.IL.LIMITP

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.IL.LIMITN 0x500A 0x5 DINT 1000:1 - RW False
AXIS2.IL.LIMITN 0x510A 0x5 DINT 1000:1 - RW False