AXIS#.MOTOR.PITCH

Description

This parameter defines the pole-to-pole pitch for a linear motor in millimeters. The pitch is the distance between two similar poles. Kollmorgen linear motors have a pitch of 32mm.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 1.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mm

Range

1 to 1000

Default Value

32

Data Type

Float

See Also

N/A

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.MOTOR.PITCH 0x500B 0x16 UDINT 1000:1 - RW False
AXIS2.MOTOR.PITCH 0x510B 0x16 UDINT 1000:1 - RW False