AXISx.OBS.KO
Description
AXIS#.OBS.KO sets the model gain of the velocity Observer.
This value represents the gain of the electro-mechanical plant of the system. The system has a high gain if it responds quickly and agilely, and this number will be high. For a heavily loaded system with a large inertia mismatch, the system does not respond quickly and is sluggish. This means the value of OBS.KO will be lower.
-
- It becomes important that OBS.KO is set correctly to ensure stability as the Observer's bandwidth In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz (AXISx.OBS.BW) is set lower.
The Observer is made up of a few components. Following is a block diagram of how the Observer is connected in the loops.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-04-03-000 |
General Information
Type |
Read/Write |
Units |
(rad/sec2)/A |
Range |
0 to 1,000,000.000 |
Default Value |
0 |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.