AXIS#.PL.AINSCALE

Description

AXIS#.PL.AINSCALE is an analog position scale factor that scales the analog input (AINx.VALUE) for AXIS#.OPMODE = 2 , AXIS#.CMDSOURCE = 3 (analog position mode).

The value entered is the motor position per 1 V of analog input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: counts/V,rad/V, deg/V, (Custom Units)/V, 16-bit counts/V

Range

+/- 4,398,046,511,104 counts/V

 

Specific unit ranges are adjusted to account for the above max count range.

Default Value

0 counts/V

Data Type

Float

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen AXIS1.PL.AINSCALE 0x500C 0x7 DINT - Position RW False
AXIS2.PL.AINSCALE 0x510C 0x7 DINT - Position RW False