AXIS#.VL.ACCFILTERED
Description
AXIS#.VL.ACCFILTERED returns the filtered acceleration.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-04-01-000 |
|
General Information
Type |
Read Only |
Description | Depends on AXIS#.UNIT.ACCROTARY |
Units |
Rotary: RPM "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component/s, RPS/s, deg/s2, (custom units)/s2, rad/s2 |
Range |
N/A |
Default Value |
N/A |
Data Type |
Float |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.