AXIS#.WS.DISTMIN
Description
This parameter sets the minimum movement that is required for commutation finding. If this value is too small, then the commutation finding might fail if too little current is used. The larger this value, the more movement is needed in order to avoid F5500 : "Wake and Shake - Insufficient movement".
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Actual position units |
Range |
0 to 90 deg |
Default Value |
1 deg |
Data Type |
Float |
See Also |
N/A |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.WS.DISTMIN | 0x5013 | 0xF | DINT | - | Position | RW | False |
AXIS2.WS.DISTMIN | 0x5113 | 0xF | DINT | - | Position | RW | False |