AXIS#.WS.IMAX
Description
This parameter defines the maximum current used for wake and shake. If the selected current is too low, the minimum required movement may not occur. If the selected current is too high, the movement may be too fast (overspeed) or too large (over maximum movement).
The maximum of this parameter is the lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK. The default value of this parameter is the half of its maximum. This value depends on the specific application.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
General Information
Type |
Read/Write |
Units |
Arms |
Range |
0 to (lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK) Arms |
Default Value |
(half of maximum) Arms |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.WS.IMAX | 0x5013 | 0xD | DINT | 1000:1 | - | RW | False |
AXIS2.WS.IMAX | 0x5113 | 0xD | DINT | 1000:1 | - | RW | False |