AXIS#.ZEROV
Description
AXIS#.ZEROV is the velocity threshold for the motor to be considered at zero velocity.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 |
|
Renamed from AXIS#.DISVTHRESH | 02-03-00-000 |
General Information
Type |
Read/Write |
Units |
Rotary: RPM "Revolutions per minute" Is a unit of frequency of rotation: the number of full rotations completed in one minute around a fixed axis. It is used as a measure of rotational speed of a mechanical component, RPS, deg/s, (custom units)/s, rad/s Linear: counts/s, mm/s, µm/s, (custom units)/s See Velocity Units for details. |
Range |
Depends on units. See Velocity Range for details. |
Default Value |
5 RPM Depends on units. See Velocity Units for details. |
Data Type |
Float |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants supported.
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | AXIS1.ZEROV |
0x5002 |
0x4 | DINT | - | - | RW | False |
AXIS2.ZEROV | 0x5102 | 0x4 | DINT | - | - | RW | False |