DIO.STATES
Description
DIO.STATES reads the states of the bi-directional IOs. Each bit corresponds to a digital state. Bit 0 = DIO1 ... Bit 5 = DIO6.
Examples
Usage
When DIO1 and DIO3 are active (DIO#.STATE = 1). Bits 0 and 2 would be set. DIO.STATES would be 5.
Code
--> DIO.STATES 5
Context
For more information see Digital Inputs and Outputs.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read Only |
| Units | N/A |
| Range | 0 to 63 |
| Default Value | N/A |
| Data Type | Integer |
| See Also | |
|
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported