DIO#.SOURCEID
Description
DIO#.SOURCEID sets the digital IO source ID, for sources that require an ID.
Examples
Usage
DIO#.SOURCEID can be used to select the compare channel whenDIO#.SOURCE = 4 (Compare).
Code
The following commands set the source of digital IO 1 to compare channel 1, and digital IO 2 to compare channel 2.
--> DIO1.SOURCE 4
--> DIO1.SOURCEID 1
--> DIO2.SOURCE 4
--> DIO2.SOURCEID 2
Context
For more information see Digital Inputs and Outputs.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
Added Compare source | 02-06-00-000 |
General Information
Type | Read/Write |
Units | N/A |
Range | 1 to 2 |
Default Value | 0 |
Data Type | Integer |
See Also | |
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported
Fieldbus Information
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable |
---|---|---|---|---|---|---|---|---|
EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen | 0x368A | DIO1.SOURCE | 0x5 | USINT | - | - | RW | False |
DIO2.SOURCE | 0x5 | USINT | - | - | RW | False | ||
DIO3.SOURCE | 0x5 | USINT | - | - | RW | False | ||
DIO4.SOURCE | 0x5 | USINT | - | - | RW | False | ||
DIO5.SOURCE | 0x5 | USINT | - | - | RW | False | ||
DIO6.SOURCE | 0x5 | USINT | - | - | RW | False |