DIO#.STATEU

Description

Gets or sets the user command state of the specified bi-directional IO when configured as a digital output (see DIO#.DIR).

Value Description
0 - Deactivated DIO#.STATE = 0, voltage removed on IO pin
1 - Activated DIO#.STATE = 1, voltage applied on IO pin

Examples

Usage

When DIO#.DIR = 1 (output) and DIO#.SOURCE = 0 (user) then the corresponding DIO#.STATEU can be set to drive the output at the IO pin.

Code

--> DIO1.DIR 1 //output
--> DIO1.SOURCE 0 //user
--> DIO1.STATEU
0
--> DIO1.STATE
0
--> DIO1.STATEU 1
--> DIO1.STATE
1

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units N/A
Range 0 to 1
Default Value 0
Data Type Integer
See Also  

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DIO1.STATEU 0x368A 0x4 USINT - - RW True
DIO2.STATEU 0x368B 0x4 USINT - - RW True
DIO3.STATEU 0x368C 0x4 USINT - - RW True
DIO4.STATEU 0x368D 0x4 USINT - - RW True
DIO5.STATEU 0x368E 0x4 USINT - - RW True
DIO6.STATEU 0x368F 0x4 USINT - - RW True