DOUT#.SOURCE

Description

DOUT#.SOURCE sets the digital output source.

Value Description
0 - User User controls the output value using DOUT#.STATEU
1 - Action Table Action table controls the output value
2 - FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Fieldbus controls the output value
4 - Compare Compare channel controls the output value

Examples

Usage

0: User controlled. DOUT#.STATE is set by DOUT#.STATEU.

1: Action table controlled. DOUT#.STATE is set by the assigned action, if any.

2: Fieldbus controlled. DOUT#.STATE is set by the fieldbus output control 3601h Digital output control sub 1.

4: Compare channel controlled. DOUT#.STATE is set by the compare channel output. The specific channel is selected by DOUT#.SOURCEID.

Code

The following commands set the source for digital output 1 to user control, and the source for digital output 2 to action table. The user is able to control the state of digital output 1, but not digital output 2.

--> DOUT1.SOURCE 0
--> DOUT1.STATE 0
--> DOUT1.STATEU 1
--> DOUT1.STATE 1
--> DOUT2.SOURCE 1
--> DOUT2.STATE 0

Context

For more information see Digital Inputs and Outputs.

Versions

Action Version Notes
Implemented 02-00-00-000

 

Added fieldbus source 02-00-01-000  
Add Sequencer source 02-02-03-000  
Added Compare source 02-06-00-000  

General Information

Type Read/Write
Units N/A
Range 0, 1, 2, 4
Default Value 0
Data Type Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

Fieldbus Information

Fieldbus Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen DOUT1.SOURCE 0x360A 0x1 USINT - - RW False
DOUT2.SOURCE 0x360B 0x1 USINT - - RW False
DOUT3.SOURCE 0x360C 0x1 USINT - - RW False
DOUT4.SOURCE 0x360D 0x1 USINT - - RW False
DOUT5.SOURCE 0x360E 0x1 USINT - - RW False
DOUT6.SOURCE 0x360F 0x1 USINT - - RW False
DOUT7.SOURCE 0x3610 0x1 USINT - - RW False
DOUT8.SOURCE 0x3611 0x1 USINT - - RW False
DOUT9.SOURCE 0x3612 0x1 USINT - - RW False