FB#.SCALED.OFFSET
Description
FB#.SCALED.OFFSET sets the offset adjustment for FB#.SCALED.P. It has the same scaling and units as FB#.SCALED.P
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-07-01-000 |
General Information
|
Type |
Read/Write |
|
Units |
Same as FB#.SCALED.P |
|
Range |
Full position range |
|
Default Value |
0.000 |
|
Data Type |
Float |
|
See Also |
|
| Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.