FB#.SCALED.POUT
Description
FB#.SCALED.POUT is the denominator of the FB#.SCALED.P scaling ratio
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-07-01-000 |
General Information
Type |
Read/Write |
Units |
N/A |
Range |
1 to 4,294,967,296 |
Default Value |
4,294,967,296 |
Data Type |
Integer |
See Also |
|
Stored in Non-Volatile Memory | Yes |
Variants Supported
All variants are supported.