REC.TRIGPARAM

Description

REC.TRIGPARAM sets the parameter the recorder uses to trigger the capture.

This parameter is not used when REC.TRIGTYPE is 0 (Immediate) or 1 (On Next Command).

The parameters that can be used with REC.TRIGPARAM are listed by REC.TRIGPRMLIST. The parameters that can be used as a trigger also have the [Trigger] tag in their DRV.HELP output.

Examples

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

N/A

Default Value

AXIS1.ILClosed "Instruction list" This is a low-level language and resembles assembly.FB

Data Type

String

See Also

DRV.HELP , REC.TRIGPRMLIST, REC.TRIGTYPE

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.