VBUS.VALUE

Description

This parameter returns the measured DC bus voltage.

Examples

Usage

The DC bus voltage measurement is used to detect unsafe operating conditions and protect the drive power electronics.

Code

--> VBUS.VALUE

159.997 [Vdc]

Context

For more information on DC bus operation and protection, refer to Power View and Regeneration.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units Vdc
Range N/A
Default Value N/A
Data Type Float
See Also VBUS.UVMODE

Stored in Non Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Parameter Index Sub-Index Data Type Float Scale Units Access PDOClosed PDO is a type of protocol frame used in some fieldbuses. A PDO contains one or more object dictionary entries, which define the application data transferred between devices. Mappable
EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen VBUS.VALUE 0x300A 0x1 DINT - - RO False