Position Loop

Overview

The position loop is active when the drive operates in position mode (AXIS#.OPMODE = 2). The parameters that govern the position loop are shown in the Position Loop view. The various types of tuning inside the drive adjust these parameters, so normally the position loop parameters do not need to be adjusted in the position loop screen.

Tabs in the Position Loop View

The position loop view includes the above active block diagram. If a block within the diagram is clicked on, the appropriate tab opens below.

Position Loop Default Behavior and Changes

By default, only a proportional gain (AXIS#.PL.KP PL.KP ) is applied in the position loop.

Position Loop Changes Based on Slider Tuning

Slider Tuning (see Slider Tuning) adjusts the proportional gain of the position loop (along with velocity loop view parameters; see Velocity Loop). If the bandwidthClosed In computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz is adjusted using the slider tuner, then when returning to the position loop screen, there will only be a change to the proportional gain. No adjustment is made to the integral gain or feedforward gain through the slider tuner. The integral saturation levels are not applicable when the integral gain is set to 0. In the Gains tab, the boxes for these values may be populated with default values whether or not the integral gain is set to 0.

Related Parameters

AXIS#.PL Parameters

AXIS#.OPMODE

AXIS#.VL.CMD