WorkBench Interface: Tool Bar

The WorkBench Tool Bar provides several convenient features.

  1. Navigation
  2. Watch Window
  3. Emergency Stop
  4. Functions
  5. Axis Control
Element FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances.
Navigation These buttons let you navigate through the history of views you have accessed, or jump up one level of nested views. See WorkBench Interface: Navigation for more information.
Watch Window This button opens the Watch window. See Watch for more information.
Panic This button immediately disables all devices.
Functions Disable drive and clear faults; save parameters to NVRAMClosed "Non-volatile random access memory" NVRAM is the general name used to describe any type of random access memory which does not lose its information when power is turned off. This is in contrast to the most common forms of random access memory today, which both require continual power in order to maintain their data. NVRAM is a subgroup of the more general class of non-volatile memory types, the difference being that NVRAM devices offer random access, like hard disks. The best-known form of NVRAM memory today is flash memory; start or disconnect communication with the selected device.
Axis Control These controls allow you to enable/disable, stop any motion, and set the axis' Command Source and Operation Mode. There are independent controls for each axis. See Axis Settings for more information.