Unwind – Registration – Rewind

4 axes with SFCClosed "Sequential function chart" It can be used to program processes that can be split into steps. The main components of SFC are: - Steps with associated actions - Transitions with associated logic conditions - Directed links between steps and transitions/STClosed "Structured text" A high-level language that is block structured and syntactically resembles Pascal and Pipe Network Motion Engine

Introduction

Machine Overview

This document details a KAS 4 axis unwind/rewind web system with a registration operation. The 4 axis are as follows:

  • Axis 1: Left Unwind/ Rewind
  • Axis 2: Draw Roller
  • Axis 3: Die Cutter
  • Axis 4: Right Unwind/Rewind
  1. Left Winder
  2. Web
  3. Draw Roller
  4. Die-Cutter
  5. Registration mark sensorClosed A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer
  6. Right Winder
  7. Distance sensors

The machine can be run bi-directionally with the left roller as the unwind axis and right roller as the rewind axis or left roller as the rewind axis and right roller as the unwind axis. All four axes are tied to a virtual master using the KAS pipe network.

The web of material contains holes in it. The rotary die cutter axis is dynamically controlled to be in sync with the holes in the web.

  1. Hole
  2. Plug

The machine is run through a Kollmorgen AKI human machine interface:

There are multiple screens in the Kollmorgen AKI performing the following functions:

  • Standby machine state
  • Manual machine sate setup and operation
  • Automatic machine state Setup and operation
  • Servo drive status and fault clearing
  • I/O status
  • Alarm awareness

Control Overview