AIN.DEADBAND
Description
AIN.DEADBAND sets the deadband of the analog input signal. When AIN.DEADBANDMODE is set to 0, and the value of the analog input is less than the value of AIN.DEADBAND, the analog command will be 0. When the analog input is greater or equal to the AIN.DEADBAND, then the analog command will be generated using the scaling specified.
When AIN.DEADBANDMODE is set to 1, the analog command is 0 if the input is less than the deadband value. When the input is greater than the deadband, the output is equal to (Input - Deadband) * Scaling. Below are illustrations of this behavior.
General Information
|
Type |
NV Parameter |
|
Units |
V |
|
Range |
0 to 12.5 V |
|
Default Value |
0 V |
|
Data Type |
Float |
|
Start Version |
M_01-00-00-000 |
Variant Support
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
5001h/0 |
M_01-00-00-000 |
Related Topics
Block Diagram for Position/Velocity Loop