AIN.OVFTHRESH
Description
This parameter defines the over voltage threshold for analog input. If AIN.VALUE is larger than AIN.OVFTHRESH, and AIN.MODE = 3 (user defined fault mode), an over voltage fault is generated.
General Information
Type |
NV Parameter |
Units |
V |
Range |
-10 to 10 |
Default Value |
10V |
Data Type |
Float |
Start Version |
M_01-13-09-000 |
Variants Supported
*In SynqNet SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
Analog Input | AIN.MODE | AIN.UVWTHRESH | AIN.UVFTHRESH | AIN.OVWTHRESH