CMPx.ARM
Description
Use this keyword to arm or disarm a Compare setpoint
Setpoint is the target value that an automatic control system, for example PID controller, will aim to reach. The setpoint value will only be compared against the Compare source (CMPx.SOURCE) if that setpoint is armed. If they match, an output pulse will be generated.
An error will be generated if CMPx.SOURCE, CMPx.MODBOUND1, CMPx.MODBOUND2, CMPx.WIDTH, and CMPx.MODEN are not set prior to enabling CMPx.ARM. If CMPx.SETPOINT is not set prior to enabling CMPx.ARM, the compare will trigger at the last set value, or the default value of 0 if the drive has been power cycled.
When accessing this keyword through a fieldbus, the values are to be interpreted as a bitmask, with each bit corresponding to one of the Compare setpoints.
Example
The following example arms setpoint 3 for CMP1.
-->CMP1.ARM 3 1
General Information
|
Type |
NV Parameter |
|
Units |
N/A |
|
Range |
Argument 1: 0 to 7 Argument 2: 0 (Disarm) or 1 (Arm) |
|
Default Value |
0 (Disarm) |
|
Data Type |
Argument 1: Integer Argument 2: Integer |
|
Start Version |
M_01-13-00-000 |
Hardware Supported
Compare functionality is supported on hardware revisions D, DB, DA, and higher depending on the drive type. Check the label on the side of the drive to ensure the AKD meets one of the following requirements.
| AKD Type | Hardware Revision Supported |
|---|---|
| AKD | Revision D or higher |
| AKD PDMM | Revision DB or higher |
| AKD-T-IC |
Revision DA or higher |
Variants Supported
*In SynqNet
SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
| Fieldbus |
Index/Subindex | Object Start Version | |
|---|---|---|---|
| 34C0h/1 |
CMP0.ARM |
M_01-13-00-000 | |
| 34C1h/1 |
CMP1.ARM |
||
Related Topics