COGCOMP.EN

Description

If the COGCOMP.EN is set to one, the current regulator will add a feedforward current depending on the actual feedback position (PL.FB ) stored in the cogging compensation correction value (COGCOMP.CORRECTIONTABLE).

General Information

This content is not applicable to KAS.

Type

NV Parameter

Units

N/A

Range

0 to 1

Default Value

0

Data Type

Integer

Start Version

M_01-14-06-001

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Index/Subindex Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

540Fh/0

M_01-14-06-001