DOUT.CTRL

Description

DOUT.CTRL sets the source of the digital outputs:

0 = Firmware controlled

1 = FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design controlled

General Information

Type

NV Parameter

Units

N/A

Range

0 to 1

SynqNetClosed SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices: 1

Default Value

0

SynqNet: 1

Data Type

Boolean

Start Version

M_01-00-00-000

Related Topics

Digital Outputs