DRV.DBILIMIT

Description

This parameter sets the maximum amplitude of the current for dynamic braking.

Example

Setting DRV.DBILIMIT to 2 limits the dynamic brake current to 2 Arms.

General Information

Type

NV Parameter

Units

Arms

Range

0 to minimum of drive peak current (DRV.IPEAK) and motor peak current (MOTOR.IPEAK).

Default Value

Minimum of drive continuous current (DRV.ICONT) and motor continuous current (MOTOR.ICONT).

Data Type

Float

Start Version

M_01-00-00-000

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

Index/Subindex

Object Start Version

EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs COE and CANopen

/0

M_01-00-00-000

Related Topics

Controlled Stop

CS Parameters

DRV.DISMODE

Dynamic Braking