DRV.DIFVAR

Description

This parameter displays all parameters which have different values than their default setting. The actual value of each parameter is directly shown after the command name and the corresponding default value is then shown in brackets.

This command also shows differences in parameters which hold a string, such as DRV.NAME.

Example

-->DRV.DIFVAR

DRV.EMUEMODE 10 (0)

DRV.NAME MyDrive(no-name)

FB1.ENCRES 0(1024)

ILClosed "Instruction list" This is a low-level language and resembles assembly.KP 50.009(24.811)

PL.KP 99.998(49.999)

VL.KP 0.108(0.000)

General Information

Type

R/O

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-05-01-000