DRV.FEATURES

Description

DRV.FEATURES returns a list of strings that describes specific features for the this firmware. The list is read only and is dependent on the firmware version. The purpose of this keywords is to activate certain views and behavior in workbench that are useful for these specific features.

Example

-->DRV.FEATURES
001: Spaces in strings
002: WS.MODE 2 Available
003: Telnet Message Grouping

Versions

Action Version Notes
Implemented M_01-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

""

Data Type

String

Stored in Non Volatile Memory

No

FieldbusClosed A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design

This keyword is not accessible via fieldbus.