DRV.RUNTIME
Description
DRV.RUNTIME returns the length of time that the drive has been running since it was first activated. This time includes the current session and the total amount of time from all previous sessions.
General Information
|
Type |
R/O Parameter |
|
Units |
Days:Hours:Minutes:Seconds |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
String |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
2011h |
M_01-00-00-000 |