DRV.VERIMAGE

Description

DRV.VERIMAGE reads the versions of the different images in the drive. This parameter returns the version data from each image .i00 file.

Example

Below is an example of the output for this parameter:

 

Kollmorgen - Digital Servo DriveClosed A servo drive is a special electric amplifier used to power electric servo motors. It monitors feedback signals from the motor and continually adjusts for deviation from expected behavior

------------------------------------

Resident Firmware: R_0-0-11

Operational Firmware: M_0-0-15

Resident FPGAClosed "Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable": FPB004_0001_00_07

Operational FPGA : FP0004_0001_00_07

 

 

General Information

Type

R/O Parameter

Units

N/A

Range

N/A

Default Value

N/A

Data Type

String

Start Version

M_01-00-00-000