FAULTx.ACTION
Description
This Parameter determines the action the drive should take when Fault 130, 131, 132, 134, 139, 451, or 702 occurs.
Parameter Value | Drive Action |
---|---|
0 | Disable Ampllifier |
1 | Ignore (fault will not be reported) |
General Information
Type |
R/W |
Units |
N/A |
Range |
0 to 1 |
Default Value |
0 |
Data Type |
Integer |
Start Version |
M_01-04-16-000 |
Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design | Index/Subindex | Object Start Version | |
---|---|---|---|
5259h/0 | FAULT130.ACTION | M_01-04-16-000 | |
525Ah/0 | FAULT131.ACTION | ||
525Bh/0 | FAULT132.ACTION | ||
525Ch/0 | FAULT134.ACTION | ||
5267h/0 |
FAULT451.ACTION | ||
525Dh/0 | FAULT702.ACTION |