FBUS.PLLTHRESH
Description
This parameter sets number of successful synchronized cycles needed to lock the PLL.
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 10,000 |
Default Value |
0 |
Data Type |
Integer, U32 |
See Also |
Appendix B: Fieldbus A Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design Manuals |
Start Version |
M_01-00-00-000 |
Fieldbus |
Index/Subindex |
Object Start Version |
---|---|---|
50B1h/0 |
M_01-00-00-000 |