IL.CMD
Description
IL "Instruction list" This is a low-level language and resembles assembly.CMD displays the q-component current command value of the current loop after any limitation (such as a parameter setting or I2t calculation).
IL.CMD is limited also by motor peak current, IL.LIMITN and IL.LIMITP .
AKD BASIC:
Change this parameter only when the motor is not moving (MOVE.MOVING = 0). If you attempt to make a change while the motor is moving, an F826, "Cannot execute during a move" fault is produced.
General Information
Type |
R/O Parameter |
Units |
Arms |
Range |
± Drive peak current (DRV.IPEAK) |
Default Value |
N/A |
Data Type |
Float |
See Also |
|
Start Version |
M_01-00-00-000 |
Related Topics
1 Current Loop