IL.DFB

Description

This parameter displays the measured, de-rotated d-component current value of the motor. This parameter is commonly used with IPM motors (MOTOR.TYPE = 6), where the d-component current is controlled for closed loopClosed The use of feedback devices (encoders, resolvers, interferometers, etc.) to allow a motor to position a user payload accurately. current regulation.

General Information

Type

R/O Parameter

Units

Arms

Range

± Drive peak current (DRV.IPEAK)

Default Value

N/A

Data Type

Float

See Also

N/A

Start Version

M_01-11-00-000