IL.FOLDFTHRESH
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.FOLDFTHRESH is the fault level of the current foldback algorithm. If IL.IFOLD drops below the value for IL.FOLDFTHRESH, then a fault is generated and the drive is disabled.
To avoid reaching the current foldback fault level, set IL.FOLDFTHRESHU well below the continuous current value for both the drive and the motor or set the IL.FOLDFTHRESHU value to zero.
General Information
|
Type |
R/O Parameter |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
Drive peak current (DRV.IPEAK) |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics
1 Current Loop