IL.MFOLDT

Description

ILClosed "Instruction list" This is a low-level language and resembles assembly.MFOLDT sets the time constant of the exponential drop (foldback) of the current towards motor continuous current.

General Information

Type

R/O Parameter

Units

s

Range

0.1 to 2,400 s

Default Value

10 s

Data Type

Float

See Also

Foldback

Start Version

M_01-00-00-000

Related Topics

Current Loop