IL.MIFOLD
Description
IL
"Instruction list"
This is a low-level language and resembles assembly.MIFOLD sets the output of the motor foldback algorithm. It is an artificial current, which can be higher or lower than the motor peak current. When IL.MIFOLD becomes lower than the existing current limit (IL.LIMITP ) it becomes the active current limit.
IL.MIFOLD decreases when the actual current is higher than motor continuous current and increases (up to a certain level) when the actual current is lower than the motor continuous current.
General Information
|
Type |
R/O Parameter |
|
Units |
A |
|
Range |
0 to 2147483.647 A |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
Foldback |
|
Start Version |
M_01-00-00-000 |
|
Index/Subindex |
Object Start Version |
|
|---|---|---|
|
/0 |
M_01-00-00-000 |
Related Topics
1 Current Loop