MOTOR.IDDATAVALID
Description
MOTOR.IDDATAVALID reports the status of the motor memory status.
The valid values for this keyword are the following:
Value |
Description |
---|---|
0 |
Error in identification |
1 |
Success in identification |
2 |
Identification in process |
3 |
Identification not started yet |
4 |
Success recognizing feedback, but failed to varify OEM "Original equipment manufacturer" A term that refers to containment-based re-branding, namely where one company uses a component of another company within its product, or sells the product of another company under its own brand. OEM refers to the company that originally manufactured the product data integrity |
General Information
Type |
R/O Parameter |
Units |
N/A |
Range |
N/A |
Default Value |
0 |
Data Type |
Integer |
See Also |
N/A |
Start Version |
M_01-02-00-000 |
Related Topics