REGEN.TESTVTHRESH
REGEN.TESTVTHRESH sets the voltage threshold for the REGEN.TEST command.
General Information
Type | Command |
Description | Sets regen test voltage threshold. |
Units | % |
Range | 1 – 99 % |
Default Value | 80 % |
Data Type | Integer |
Start Version | M_01-18-06-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | Yes |
AKD with Position Indexer | Yes |
AKD EtherCAT ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs | Yes |
AKD CANopen | Yes |
AKD BASIC | Yes |
AKD SynqNet SynqNet is a digital machine control network. Built on the 100BT physical layer, SynqNet provides a synchronous real-time connection between motion controllers, servo drives, stepper drives, I/O modules, and custom devices | Yes* |
AKDEtherNet/IP | Yes |
AKD Profinet | Yes |
AKD sercos® III | Yes |
AKD-N | No |
AKD-C | Yes |
Fieldbus Information
If your drive type is listed as supported but no index, address, or instance number is listed, then this parameter is accessible through WorkBench, but not over your fieldbus type.