TEMP.CONTROL
Description
Reads the temperature of the control board temperature sensor A sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer.
General Information
Type |
R/O Parameter |
Units |
Degrees Celsius |
Range |
-127 to 128 |
Default Value |
N/A |
Data Type |
Integer |
Start Version |
M_01-09-00-000 |
Related Topics